Technical FAQs

Ask a Question

Can vertical cable managers be installed inside of the finger style cable managers, like AR7580A, AR7585 or AR7588? If so, what options are there?

Issue: 
A customer want to install secondary cable management inside of the vertical cable management fingers. 

Product Line: 
NetShelter SX

Environment: 
All models, all serial numbers. 

Cause: 
Customers may wish to manage cables inside of the finger style cable managers. 

Resolution: 
  
See attached file
Was this helpful?
What can we do to improve the information ?