Technical FAQs

Ask a Question

Video: How to Clear Alarms on an InRow ACRD200 Cooling System

How Clear Alarms on an ACRD200 Cooling Unit

Product line: 
InRow Cooling Products ACRD200

All Serial Numbers

Install, Configuration


First you need to access the Clear Alarms menu you can do this by hitting the <ESC> until visible
Then select ENTER
It will ask if you want to clear alarms select yes
You will be prompted for a Password
Use the default password of “apc”
If this does not work check with your Admin for the correct password
If password has been lost use the last eight digits of the serial number
Now select clear alarms again and again select yes and alarms will be cleared.
Was this helpful?
What can we do to improve the information ?