Technical FAQs

Ask a Question

Can vertical cable managers or 0U accessory rails be installed in the front and rear of a NetShelter SX cabinet?

Customers want to know if there is flexibility in installing vertical cable managers or where to mount the 0U accessory rails.

Product Line:
NetShelter SX Vertical Cable Management

All versions and serial ranges.

Owner's Manuals show cable managers and 0U accessory rails installed in specific areas of the cabinet.

The 0U accessory rails that come preinstalled in the rear of the SX cabinet can be moved to the front. So, anything that attaches to that rail can also be mounted in the front of the cabinet.
Vertical cable managers that attach to the SX cabinet's vertical mounting rails can be installed to the front or rear rails.

Was this helpful?
What can we do to improve the information ?