Technical FAQs

Ask a Question

Data Center Expert | How do I access the built-in network troubleshooting tools?

Issue:
Troubleshooting tools for StruxureWare Data Center Expert.

Product Line:
StruxureWare Data Center Expert (DCE)

Environment:
StruxureWare Data Center Expert (all versions)

Cause:
Troubleshooting issues such as connections and communications with devices or servers, at times, requires more tools than are available within the Data Center Expert desktop client.

Resolution:
 
1) Navigate to the web interface of DCE by entering the IP address or hostname into a web browser.
NOTE: If Data Center Expert is restricted to HTTPS only, you will need to specify https as part of the URL.

2) Log into the web interface and then select Status in the upper right.

3) Under Additional Information, select Troubleshoot Network from the drop down menu and then select Submit.
 
4) Under Function, select one of the available utilities, which are listed below:
  • Ping
  • Trace Route
  • Resolve Host
  • Netstat
  • IP Information
Was this helpful?
What can we do to improve the information ?