Technical FAQs

Ask a Question

Ping Response ICMP Traffic- there are no configuration options to turn off ICMP responses from the 300/303/310/400 series appliances

Issue:

Can Ping Response (ICMP Requests) Be Disabled on NetBotz Version 1 Appliances?

Product Line:

NetBotz

Environment:

NetBotz version 1

Cause:

The ping response (ICMP traffic) can not be turned off on NetBotz Appliances

Resolution:

There are no configuration options to turn off ICMP responses from the 300/303/310/400 series appliances
 
Was this helpful?
What can we do to improve the information ?