Technical FAQs
Technical FAQs
The following OID will request information about FM40 AC Coil Temperature:
.iso.org.dod.internet.private.enterprises.apc.products.hardware.airConditioners.airFM.airFMSystem.airFMSysStatus.airFMSysCoilFluidTempC
1.3.6.1.4.1.318.1.1.13.1.4.1.5.0
It is recommended to pull this OID from the unit that is selected for priority scanning by adding it as a supplemental OID. To do so please go into context menu and select :
Settings - SNMP Device Settings - Supplemental OIDs.
"