Technical FAQs

Ask a Question

AP9635 Modbus registers are not compatible with NAM Galaxy 5000 Modbus registers

 
 
Issue:
AP9635 Modbus registers are not compatible with NAM Galaxy 5000 Modbus registers.
 
 
Product line:
Galaxy 5000 NAM
 

Environment:
Galaxy 40KVA, 50KVA,60KVA, 80KVA, 100KVA and 130KVA
 

Cause:
AP9635 Modbus registers are not qualified for NAM Galaxy 5000.
 
 
Resolution:
Do not use AP9635 MODBUS resistor for NAM Galaxy 5000 UPS.
 
Use below link to download the correct Modbus register used for NAM Galaxy 5000.
 
http://www.apc.com/shop/us/en/products/MGE-JBus-Modbus-Card/P-66061
 
 
 

 
Was this helpful?
What can we do to improve the information ?