Technical FAQs

Ask a Question

Video: How to change a Network Air FM from Metric to Standard US measurements

Issue:
How to change a Network Air FM from Metric to Standard US measurements.
 
Product line:
FM 35-50, IR40, ACFM400, ACFM200.
 
Environment:
All Serial Numbers.
 
Cause:
Install, Configuration.
 
Resolution:

 
  1. How to change a Network Air FM from Metric to Standard US measurements.
  2. Press the ESC Key until you get to the main menu.
  3. Press ENTER on Setup.
  4. Press ENTER on System 1.
  5. Press ENTER on Display.
  6. Press ENTER on Temp\Pressure Units.
  7. Press ENTER on Temp Units and now you will need to enter a password.
  8. The default password is 7852 Select each number and then press ENTER to move to the next one.
  9. Press ENTER on Temp Units again.
  10. Now you have the option to change between Celsius and Fahrenheit.
  11. Press ENTER after changing.
  12. Press the DOWN arrow and then ENTER to change the Pressure.
  13. Now you have the option to choose between English and Metric.
  14. Finish by pressing the ENTER key and then press ESC until you get to the status menu.
Was this helpful?
What can we do to improve the information ?