Technical FAQs

Ask a Question

NetBotz 200 and 250 must be discovered as an SNMP device in StruxureWare DCE.

Issue:

NetBotz 200 and 250 does not discover when choosing NetBotz discovery in StruxureWare Data Center Expert (DCE).

Product Line:

NetBotz
StruxureWare Central / DCE

Environment:

NetBotz 200 / 250 discovery in StruxureWare DCE

Cause:

The NBRK0200 and the NBRK0250 are based on technology from the earlier APC Environmental Monitor. This was similar to the Network Management cards in other APC devices. NetBotz 300, 400, and 500 series units are discovered using HTTP or HTTPS based on individual configuration.

Resolution:

Because the code in the NetBotz 200 and 250 is not the same as the 300, 400, and 500 series NetBotz appliances, it must be discovered as an SNMP device in StruxureWare DCE. It can not be discovered using HTTP or HTTPS in DCE.
 
Was this helpful?
What can we do to improve the information ?