MONGOLIA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Audio-Video Solutions
AV Surge Protectors
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
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
Data Center Assessment Services
Install
Installation Services
Operate
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
MONGOLIA - Choose Country or Region
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
What materials are used in the main structure and acoustic foam lining of the NetShelter CX?
Issue:
From what materials is the NetShelter CX is constructed?
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
Environmental
Resolution:
The NetShelter CX is constructed using Melamine Faced Chipboard (MFC).
The NetShelter CX also uses a combination of Medium Density Fibre Board (MDF) and High Pressure Laminate (HPL) on its top and MDF on its plinth base.
The four acoustic foams & barriers which line the interior of the CX are:
Foam 1. Meets HF1 the highest rating for cellular foam products.
Foam 2. FT70 - flame retardant, compliant to BS476 part 6 ; class O, and cellular part 7: class 1, UL94-HF1 and UL94-VO and F.M.V.S.S 302
Foam 3. FT80 - flame retardant, compliant to BS476 part 7: class 1, UL94-HF1 and UL94-VO and F.M.V.S.S 302
Rubber. CB-V0-02