NetBotz location information not retained on Pelco camera after reboot.
Issue:
NetBotz location information not retained on Pelco camera after reboot.
Product Line:
NetBotz
Pelco Cameras
Environment:
Botzware version 4.2 and lower that support Pelco cameras
Cause:
In NetBotz Advanced View, you are able to put specific location information to the NetBotz appliance, all of it's pods, and it's sensors. In the case of a Pelco camera, you can also add the camera to the NetBotz appliance as a shared pod.
We have seen that during a reboot, this location information is not retained for the Pelco camera only. You can re-add this information but it will again be lost on subsequent reboots.
Resolution:
This is resolved in Botzware version 4.3