Technical FAQs

Ask a Question

Wrong status if wrong sensor is plugged into sensor port on Netbotz Rack Monitor 550 with an Internal SP150

Issue:

Wrong status if wrong sensor is plugged into sensor port on Netbotz Rack Monitor 550 with an Internal SP150

Product Line:

NetBotz

Environment:

NetBotz version 3 appliances and sensors

Cause:

In some instances, sensors can be connected to only specific sensor ports.

Resolution:

"The attached XL sheet lists all the issues that may be seen if the wrong sensor is plugged into a port on the Netbotz 550.

This attachment references the following sensors:
Temp
Temp / humidity
Smoke
Vibration
0-5 volt cable
Spot leak
Rope Leak
Beacon
Dry contact
Ethernet
Door
A-Link


plugged into the following ports:
Universal Sensor port 1-6
Rope port
Beacon port
Ethernet port
A-Link port
Was this helpful?
What can we do to improve the information ?