Technical FAQs
Technical FAQs
The Symmetra RM's input voltage must also be 208VAC if being used with the SYTF2. Even though the Symmetra RM has the ability to output 208VAC when receiving 240VAC from Utility power, anytime the Symmetra RM is put into BYPASS Mode the UPS will not be able to condition the output power to put out 208VAC. If the UPS has 240VAC on the input side and is put into Bypass mode, it will then pass that voltage through the UPS to the output. This will cause the SYTF2 to be receiving 240VAC and therefore it will only be able to step it down to approximately 139VAC.
Resolution