Technical FAQs

Ask a Question

Power distribution panels available for Symmetra LX, International models

"The following power distribution panels are available:

SYPD4 - (2) IEC320C19, (8) IEC320C13
SYPD8 - (4) IEC320C19
SYPD10 - (1) IEC309, (2) IEC320C19
"
Was this helpful?
What can we do to improve the information ?