Technical FAQs

Ask a Question

Is there a blank NetShelter door badge available? If so, what size is available and how many are in the package?

Issue: 
Customers may want to have their logo on the cabinet. 

Product Line: 
NetShelter SX

Environment: 
All models, all serial numbers. 

Cause: 
Customers may not want the APC by Schneider Electric logo on their cabinets, or may want additional badges. 

Resolution: 

We offer sku AR7001X384. This is a pack of 40 door badges, 
The door badge is oval.
The dimensions are: 71.5 mm wide x 39.4 mm high. 
Was this helpful?
What can we do to improve the information ?