Technical FAQs

Ask a Question

Video: How to change a Cooling Set point on a push button Uniflair display

Issue:
How to change a cooling set point on a Uniflair Unit
 
Product line:
All Uniflair Units with Push-Button Display, All Chilled Water Uniflairs.
 
Environment:
All Serial Number with Push-Button Units
 
Cause:
Repair, Install, Maintenance
 
Resolution
 
How to change a Cooling Set point on a push button Uniflair display
 
Press <> PRG
 
Settings Menu <> ENTER
 
Code <> 00000 ENTER
 
Operative settings <> ENTER
 
Press ENTER again to the cooling set point
 
Use the Arrows to set the correct temperature.
 
Press ENTER twice and then ESC back out to the main menu
 
 
 
Was this helpful?
What can we do to improve the information ?