You can select to enable or disable alarm notifications to define if you want to be notified of new alarms.
There are two types of alarm notifications:
A generic alarm notification from Standard devices.
Alarms are bundled and sent every five minutes.
An instant push notification on critical alarms occurring on Premium devices.
When a critical alarm occurs on a Premium device, it will automatically create an incident. You can access the incident from the notification or from the Incidents tab in the app.