Which brackets should be used to install a NetShelter SX into a IBC High Seismic Area?
Issue:
The customer needs a mounting bracket for a NetShelter SX cabinet that's rated for installation in a IBC High Seismic Area.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
A customer needs to install a NetShelter SX cabinet into an IBC High Seismic Area.
Resolution:
AR7701A-S is rated for NetShelter SX cabinets to be mounted in an IBC High Seismic Area. The Structural Calculations For Seismic Anchorage document is being updated to reflect this.
AR7701A-S replaces both AR7701-S and AR7701 in IBC High Seismic Area installations.
Do not use the AR7701 in an IBC High Seismic Area installations of NetShelter SX cabinets.
For cabinets installed in an IBC Low Seismic Area or Moderate Seismic Area the included pallet bracket or AR7701 can be used to mount the cabinet.