Technical FAQs

Ask a Question

In Hyper-V, Virtual Machine shutdown is delayed when VM Migration is enabled.

There is a delay proceeding with virtual machine shutdown when VM migration is enabled for Hyper-V.

Product Line:
PowerChute Network Shutdown v3.1 and above

Windows Hyper-V

If the VM Migration time is insufficient in attempting to migrate all VMs, there is a timeout issue before PowerChute proceeds with shutting down VMs that failed to migrate.

Ensure you allow sufficient time for the the VM migration duration to attempt to migrate all VMs.
Was this helpful?
What can we do to improve the information ?