Technical FAQs

Ask a Question

What is the maximum number of ACRD units that can be grouped together in group control mode?

Issue:
What is the maximum number of ACRD units that can be grouped together in group control mode?

Product line:
ACRD100, ACRD101, ACRD200, ACRD201

Environment:
Data Center Cooling

Cause:

Resolution:
12 is the maximum number of units that can be grouped in one group.
 
Was this helpful?
What can we do to improve the information ?