Technical FAQs

Ask a Question

Can I use the Pod Sharing functionality of NetBotz devices with Scanned devices?

Issue:

Pod Sharing functionality of NetBotz devices with SNMP Scanned devicesnot an option.

Product Line:

NetBotz
StruxureWare Data Center Expert
Environment:

Netbotz device crawlers or SNMPscanners.

Cause:

Scanned devices or Device Crawlers in older NetBotz appliances can not be used with the NetBotz pod sharing functionality.

Resolution:

It will be necessary to directly connect to the appliance that is monitoring the SNMP device to view this on a NetBotz web page or using Advanced View. StruxureWare DataCenter Expert can see this information.
 
Was this helpful?
What can we do to improve the information ?