Technical FAQs

Ask a Question

System reports 100% CPU usage for java running PowerChute Business Edition agent 8.5 on SuSE 10 with SP1 or SP2 installed.

Issue:
System reports 100% CPU usage for java running pcbe agent 8.5 on SuSE 10 with SP1 or SP2 installed.

Product Line:
PowerChute Business Edition agent 8.5

Environment:
SuSE 10 with SP1 or SP2

Cause:
This can occur if the config.sh file is run more than 1 time.

Solution:

To resolve the problem stop the APC PBEAgent service and reboot the system.

Note: This issue has been fixed in the release of PCBE 9.0
Was this helpful?
What can we do to improve the information ?