Technical FAQs

Ask a Question

OID Information for External Humidity Sensor on Version 1 Appliances

Issue:

OID Information for External Humidity Sensor on Version 1 Appliances

Product Line:

NetBotz

Environment:

NetBotz version 1 and SNMP

Cause:

The OID information for the NetBotz External Humidity Sensor is all in the published MIB under:
iso.org.dod.internet.private.enterprises.netBotz.ExpPortTable.expPortEntry.expPort-ext-humi

Resolution:

The OID information for the NetBotz External Humidity Sensor is all in the published MIB, under iso.org.dod.internet.private.enterprises.netBotz.ExpPortTable.expPortEntry.expPort-ext-humi.

The OIDs map to:
.1.3.6.1.4.1.5528.31.1.80.1.0 (for External port 1)
.1.3.6.1.4.1.5528.31.1.80.2.0 (for External port 2)
.1.3.6.1.4.1.5528.31.1.80.3.0 (for External port 3)
.1.3.6.1.4.1.5528.31.1.80.4.0 (for External port 4)
.1.3.6.1.4.1.5528.31.1.80.5.0 (for External port 5)
.1.3.6.1.4.1.5528.31.1.80.6.0 (for External port 6)
.1.3.6.1.4.1.5528.31.1.80.7.0 (for External port 7)



Was this helpful?
What can we do to improve the information ?