Technical FAQs
Technical FAQs
(2) L5-20R (3-pin twist-lock)
(1) L14-30R (4-pin twist-lock)
The L5-20R outlets provide single-phase 100, 110, or 120v AC (Phase-Neutral) service. These outlets are sourced consistently from specific phases (legs) on the Symmetra LX.
The L5-20R located on the left of the SYAPD1 PDU Panel sources from Phase 1.
The L5-20R located on the right of the SYAPD1 PDU Panel sources from Phase 2.
The UPS is capable of displaying the load on each phase; this information can be accessed either via the front LCD display or via the included network management card. The information in this document, in addition to the load percentages given by the UPS display, should be enough to balance the load properly across the output phases.