Technical FAQs

Ask a Question

InRow RC Standard and Optional Features

"1-The Standard Features of the InRow Rc Coolling Unit are as follow:

Variable Speed Fans
Shutdown Input/Alarm Output
Chilled Water Flow Meter
2-way/3-way Floating Point Valve
Dual A-B Power Feed
Washable Filter
Pipe Adapters
Top or Bottom Piping
Condensate Pump with Dual Float Switches
Network Management Card
Remote Temp Sensor
Microprocessor Controller

2-Other Optional Features or accessories are as follow:

Cable Leak Detector
Baying Kit InRow RC to NetShelter VX rack
30% ASHRAE 52.1 Filter (MERV 8 per ASHRAE 52.2)
NetShelter SX Height Adapters
NetShelter VX Height Adapters
Power Trough (Overhead power distribution between racks)
Data Partion Trough (Allows removal of RC unit without disrupting cabling)

"
Was this helpful?
What can we do to improve the information ?