Can I use the NetBotz leak rope sensors with the Network Air units?
Issue:
NetBotz leak rope sensors can not be used with Network air units.
Product Line:
NetBotz
Environment:
NetBotz version 3 and leak rope sensors NBES0308 and NBES0308
Cause:
NetBotz leak rope sensors NBES0308 and NBES0308 have specific resistances that are expected by the NetBotz appliance.
Resolution:
The leak rope sensors AP9325 and AP9326 are designed specifically for the APC Network Air units they work with, You can not use these sensors on a NetBotz appliance nor can you use the NetBotz NBES0308 and NBES0308 rope leak sensors with APC's Air units.