Technical FAQs

Ask a Question

BMS AP9921X-AP9922; alarms “Battery High User Defined Voltage”

 
 
 
Issue:
BMS AP9921X-AP9922; alarms “Battery High User Defined Voltage”

 
Product line:
Battery Management System (BMS) AP9921X & AP9922

 
Environment:
All models, all serial numbers

 
Cause:
The voltage of a battery is above the configured threshold.

 
Resolution:
If a specific battery causes repeated alarms (especially if the alarms have increasing deviation percentages), the battery is failing. Replace the battery.
 
 
 
Was this helpful?
What can we do to improve the information ?