Technical FAQs

Ask a Question

Server Access options are blank on StruxureWare DCE Desktop Client after upgrade to v7.5.0

 

Issue:

Server Access options are not visible after upgrading to v7.5.0



Product Line:

StruxureWare Data Center Expert

Environment: 

Version 7.5.0

Cause:

It has been seen that after upgrading systems to v7.5.0, the Server Access options are blank if HTTP had been disabled prior to the upgrade. 

Resolution:

In order for this to be corrected, you must contact your local Technical Support for StruxureWare Data Center Expert. A remote session may be required to resolve this issue.
In the meantime, if you have a recent backup from prior to the upgrade, you may want to restore that backup to the server.
Was this helpful?
What can we do to improve the information ?