LIBYA - Choose Country or Region
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
LIBYA - Choose Country or Region
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
Video: How do I create/restore a configuration backup on a v3 NetBotz Appliance?
Issue:
Process for creating and restoring a backup on a v3 NetBotz Appliance.
Product Line:
NetBotz version 3
Environment:
NetBotz Model: 355, 455, 450, 550, or 570.
Resolution:
NOTE:
A backup from a NetBotz Appliance can only be restored on the same appliance. For details see knowledge base
FA176136
.
Creating a Backup
1) Log into the
Advanced View
application using an Administrator account.
2) Select the
Configuration Tab
and then under Appliance Settings select
Backup
.
3) Click
Browse
to select a drive and directory in which to store the backup file. Click
OK
to return to the Appliance Backup window.
4) If you would like the backup to be password protected, type a password in the
Password
and
Verify Password
fields.
5) Click
OK
and the backup will be saved to the location specified in step 3.
Restoring a Backup
1) Log into the
Advanced View
application using an Administrator account.
2) Select the
Configuration Tab
and then under Appliance Settings select
Restore
.
3) Click
Browse
and navigate to the backup file location. Click
OK
to return to the Appliance Restore window.
4) If you set a password for the backup when creating it, enter the password in the
Password
field.
5) Click
OK
and the backup will upload to the appliance. The Appliance will reboot and restore the backup.