Technical FAQs

Ask a Question

Can the Combination Lock Handle or PX-HID Lock be installed onto the ARU?

Issue:
Customer requests compatibility information between the Combination door handle or PX-HID lock, and the ARU.

Product Line:
NetShelter SX ARU, NetBotz PX-HID

Environment:
All versions and serial ranges.

Cause:
Customer requires secure access to the ARU.

Resolution:
The Combination Lock Handle and PX-HID Lock are not compatible with the ARU.
Was this helpful?
What can we do to improve the information ?