Technical FAQs

Ask a Question

What is the NMFC item number and freight class for NetShelter cabinets?

Issue:
Customers may need to know the NMFC item number and freight class for NetShelter cabinets.

Product Line:
NetShelter SX, SV, CX, WX, VX

Environment:
All versions and serial ranges.

Cause:
This information is required for common standardized freight pricing.

Resolution:

The following information is consistent for all unpopulated cabinets.
NMFC Item 63160 for Electrical Enclosure
Freight Class 125

 
Was this helpful?
What can we do to improve the information ?