Technical FAQs

Ask a Question

What to do if PowerChute Network shutdown configuration wizard displays blank Network Configuration page?

Issue:
After installing PowerChute Network Shutdown when the configuration wizard runs the PowerChute Setup: Network Configuration page display is blank.

Product:
PowerChute Network Shutdown version 3.1

Environment:
All supported Windows OS

Cause:
Corruption in pcnsconfig.ini

Solution:

1 - stop PowerChute service
      Open command prompt as administrator and type net stop PCNS 1

2 - Open pcnsconfig.ini using wordpad or notepad
      The default path to pcnsconfig.ini is C:\Program Files\APC\PowerChute\group1

3 - Enter the system ip information to [Networking] localHostAddress = for IP v4 or UnicastAddress = for IP v6

[Networking]
protocol = https
httpPort = 3052
httpsPort = 6547
NetworkConfig = IPV4
ESXiVirtualInstall = false
HyperVVirtualInstall =
MulticastAddress =
IPv6NetworkConfig = unicast
localHostAddress = 192.168.1.X
UnicastAddress =


4 - Add user name, password, and NMC IP information to [NetworkManagementCard]

[NetworkManagementCard]
mode = single
IP_1 = 192.168.0.X
port = 80
protocol = http
enrolWithNMC = true
acceptCerts = false
username = apc
password = apc


NOTE: user name and password are not visible. You need to enter username = along with password =. This information will be read and deleted from the ini file when the service is started. See Knowledge Base document FA159758 for assistance with PCNS user name and password. If port has been changed from 80 and protocol has been changed they will need to be adjusted accordingly.

5 - Restart PowerChute service
     from command prompt type net start PCNS1

6 - After restarting PCNS1 service log into PCNS web page and select Shutdown Settings to complete the configuration.

 
Was this helpful?
What can we do to improve the information ?