Technical FAQs

Ask a Question

How does the modulation of the electric heaters work on an ACRP unit?

Issue:  
How does the modulation of the electric heaters work on an ACRP unit?

Product line:
ACRP1XX, ACRP5XX

Environment:  
All Serial Numbers

Cause:  
Install, Repair

Resolution:
Each heater is turned on as needed so the CW unit has three stages: 33.33%, 66.66%, and 100%. The DX unit has two stages: 50% and 100%.
 
 
 
Was this helpful?
What can we do to improve the information ?