NetBotz v4.2 Web Client Does Not Run on IE8 or IE9 in Compatibility View
Issue:
The NetBotz version 4.2 Web Client does not run on Internet Explorer 8 or Internet Explorer 9 when displayed in Compatibility View.
Product Line:
NetBotz
Environment:
Microsoft Internet Explorer version 8.0
Microsoft Internet Explorer version 9.0
NetBotz version 4.2 Web Client
Cause:
It is a known issue that the NetBotz v4.2 Web Client does not function with the browser set to display websites in Compatibility View.
Resolution:
Change the Compatibility View Settings in the browser.
For more information about Compatibility View, see the following Microsoft article: http://blogs.msdn.com/b/askie/archive/2009/03/23/understanding-compatibility-modes-in-internet-explorer-8.aspx
This issue should be resolved with the release of 4.3