Ports used on ISX Central / StruxureWare Data Center Expert
Issue:
Ports used on InfraStruxure Central
Product Line:
InfraStruxure Central
StruxureWare Data Center Expert
Environment:
InfraStruxure Central any version
StruxureWare Data Center Expert any version
Cause:
Network usage.
Resolution:
The following outlines ports used and their application on any ISX Central Server:
Note: Ports or Protocols preceded by * can be changed from their default port number.
Incoming:
Port 80 (TCP/UDP) - *HTTP Communication from NetBotz Appliances / *ISX Central Console/Web API and 3rd party integrations.
*Port 443 (TCP) - HTTPS Communication from NetBotz Appliances / ISX Central Console
*Port 161(UDP), 162 (TCP/UDP)- SNMP Communication from SNMP Agent
*Port 502 (TCP/UDP)- Modbus TCP Communication from Modbus Device/Gateway Outgoing:
Port 80 (TCP/UDP)- *HTTP Communication to NetBotz Appliances / *ISX Central Console / HTTP Post to Web Server/Web API and
3rd party integrations.
*Port 443 (TCP) - HTTPS Communication to NetBotz Appliances / ISX Central Console
*Port 161 (UDP), 162(TCP/UDP) - SNMP Communication to SNMP Agent
*Port 25 (TCP)- SMTP Communication to Email Server
Port 21 (TCP)- FTP Communication to FTP Server
Port 123 (UDP)- NTP Communication to NTP Server
Port 139 (TCP/UDP)- SMB Communication to NAS / SAN
Port 53 (TCP/UDP)- DNS Communication to DNS Server
Port 111 (TCP)- NFS Mount
Port 2049 (UDP)- NFS Communication to NAS / SAN
Port 6000 (TCP)- APC Proprietary Communications protocol for use with AP76xx outlet strips and gen1 PDU on private lan.
Port 445 (TCP)- CIFS Communication to NAS / SAN
Port 502 (TCP/UDP)- Modbus TCP output to Building Management System
*Port 389(TCP/UDP)- Active Directory/LDAP