Technical FAQs

Ask a Question

Camera Specifications for 300/303/310/400

Issue:

Camera Specifications for 300/303/310/400

Product Line:

NetBotz

Environment:

NetBotz version 1

Cause:

Camera specifications.

Resolution:

Camera Specifications for 300/303/310/400:


-All cameras feature an 87 º lens, with resolution no less than 350 x 280 pixels.

-The lens is 15 º adjustable at any direction on all models except the WallBotz 300.

-Saved images are time/date stamped.
Was this helpful?
What can we do to improve the information ?