Technical FAQs

Ask a Question

This document describes the altitude derating factor of the SUVT

"

Yes it does: The Maximum installation with no derating of the UPS output shall be 3280 feet (1000m) above sea level. At higher altitudes the following derating shall apply:

a. 1500 m derating factor of .95

b. 2000 m derating factor of .91

c. 2500 m derating factor of .86

"
Was this helpful?
What can we do to improve the information ?