Technical FAQs
How can I mass configure an Network Management Card (NMC) or NMC embedded product?
Issue
How can I mass configure or configure multiple Network Management Card devices?
Product Line
- Network Management Card 1 (NMC1) - AP9617, AP9618, AP9619
- Network Management Card 2 (NMC2) - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/AP9635CH
Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products.
- Older products such as the AP9605, AP9606 and related products (ie. AP9312TH, Masterswitch 1/2) do not have this feature.
Environment
- All serial numbers
- Firmware versions AOS v2.5.0 or higher
For users that have multiple APC Network Management Cards or devices with an embedded Network Management card, mass configuration of those devices can greatly ease administration. These instructions will provide defaults on downloading and uploading a single configuration file (config.ini) as well as downloading and uploading multiple files at a time with the intent of 'pushing' these files to different devices in an automated fashion.
These instructions will also include notes for Network Management Card 2 users wishing to push .csf script files for user management within v6.X.X firmware and higher.
Resolution
Refer to the individual sections below depending on what you'd like to do.

How do I obtain a config.ini file from a single Network Management Card?
For all firmware versions, one option is to retrieve the config.ini file via FTP from the Network Management Card(NMC) device (or SCP if enabled). Steps for Windows FTP are provided below:
- Open a command prompt and type: ftp<space><ip address of the NMC>
- Log into the NMC device using your login credentials.
- Type "bin" for binary mode and "hash" for hash marks (optional) indicating the transfer is in progress.
- Once logged in, type get<space>config.ini.
- Once finished, type "bye" and you will exit from the NMC device.


Once the config.ini file is downloaded via either method, you can open it and view all settings from the NMC device.
How do I upload a modified manipulating to a single Network Management Card?
To upload a modified config.ini file, you can follow a couple of different methods.
Method 1 - via Web UI
Note: The five steps below apply to devices with v3.X.X and v5.X.X firmware.
- Open a web browser and go to the IP address or hostname of the NMC device.
- Log into the NMC device.
- Once logged in, go to Administration Tab->General->User Config File.
- From this menu, you will need to browse for the config.ini file that you wish to upload.
- Once you have located the file, press Apply and the file will be uploaded.

Note: The five steps below apply to devices with v6.X.X firmware.
- Open a web browser and go to the IP address or hostname of the NMC device.
- Log into the NMC device
- Once logged in, navigate to Configuration->General->User Config File.
- From this menu, you will need to browse for the config.ini file you wish to upload.
- Once you have located the file, press Apply and the file will be uploaded.

Method 2 - via FTP
- Open a command prompt and type: ftp<space><ip address of the NMC>
- Log into the NMC device using your login credentials.
- Type "bin" for binary mode and "hash" for hash marks (optional) indicating the transfer is in progress.
- Once logged in, type put<space>config.ini.
- Once finished, type "bye" and you will exit from the NMC device.
How do I configure multiple devices at once using config.ini?
In some cases, a user may wish to upload a config.ini file to several devices, in an attempt to minimize workload and configuration time. APC by Schneider Electric offers a couple of methods to upload configurations to several devices at one time.
Method 1 - ISX Manager - Discontinued Product
ISX Manager offers a mass configuration utility. Please reference the user's manual or Help guide for the ISX Manager for information on performing the mass configuration.

Method 2 - InfrastruXture Central/StruxtureWare Central/StruxureWare Data Center Expert
StruxureWare Data Center Expert offers a mass configuration utility. Please reference the user's manual or Help guide for the StruxureWare Data Center Expert for information on performing the mass configuration any important limitations..
Note: The mass configuration option in StruxureWare uploads specific settings designated by the StruxureWare application. Therefore, not all settings may be applied, and some settings that shouldn't be applied, may be uploaded. It is recommended that this feature only be used for devices of the same type. ie. Smart UPS to Smart UPS, Switched Rack PDUs to Switched Rack PDUs.
Method 3 - INI Utility
APC by Schneider Electric offers a free program called the INIUtility. This program allows the user to download and modify one config.ini file and then upload it to several different NMC devices. It is available as an attachment to this knowledge base. v3 of this utility also supports pushing/uploading .csf files, as outlined in knowledge base FA176542, for v6.X.X Network Management Card 2 devices for mass configuration of user management. (This file is for upload only.)
You should have (5) files once the utility is uncompressed:
- download_list.txt
- iniutil.exe
- ReadMe.txt
- upload_list.txt
- winftp32.dll
You will need to save your config.ini (or .csf script) file that you wish to upload (if you've already modified it) to this same directory, If you have not downloaded it manually, you can use the iniutil.exe utility and download_list.txt files to perform a mass download of config.ini.
The download_list.txt and upload_list.txt files can be edited with the IP address, INI file to be downloaded/uploaded, and login credentials. You must un-comment each field (by removing ; at the beginning of each line) in the files to have the program run properly. Below is an example of each file at a default and modified state.
Please note .csf files are upload only as user credentials are not downloadable for security reasons.
Default:
;SystemIP=168.192.0.1
;IniFileName=config.ini
;SystemUserName=apc
;SystemPassword=apc
Modified:
SystemIP=192.168.1.1
IniFileName=config.ini
SystemUserName=apc
SystemPassword=apc
Note: Notice the ' ; ' has been removed from each line in the modified example. If you leave this character in the text file, it will comment the lines out and this procedure will not work. Make sure to remove the character as shown in the modified example.
Each list can also be modified with multiple NMC devices. Below is an example of the list:
SystemIP=192.168.1.1
IniFileName=config.ini
SystemUserName=apc
SystemPassword=apc
SystemIP=192.168.1.2
IniFileName=config.ini
SystemUserName=apc
SystemPassword=apc
SystemIP=192.168.1.3
IniFileName=config.ini
SystemUserName=apc
SystemPassword=apc
In this case, all three devices will either download or upload the config.ini files. The user can edit their config file to meet their requirements.
Note: If you are only uploading a couple of settings, it is advised that you cut the section you would like and paste it into a different .ini file. ie. SNMP section can be copied into the snmp.ini file. On upload, only the SNMP settings will be parsed into the NMC device. In this case, you would modify the upload_list.txt to the following:
SystemIP=192.168.1.1
IniFileName=snmp.ini
SystemUserName=apc
SystemPassword=apc
Once you have the config.ini file that you would like to upload to your multiple devices and your upload_list.txt has been updated with all devices, then you can start the upgrade.
Doubleclick on the "iniutil.exe" program. You should see the following:
INI Utility.
*****************************************************
1. Upload configuration file
2. Download configuration file
3. Exit
Action:
To upload the config.ini file, select option 1. You will then see the following:
Action: 1
Batch upload file upload_list.txt found
1: Use parameters in batch file
2: Enter new parameters for single upload
3: Exit
Action:
Select option 1 and this will reference the upload_list.txt file for the NMC devices you wish to upload. A successful upload should appear with Successful next to each step. Any step that does not, you should check. ie. Logging in - Unsuccessful. You should check the login credentials.
For further information on this, read the ReadMe document included in the download.