User Access Levels for Version 1 Netbotz Appliances
Issue:
User Access Levels for Version 1 Netbotz Appliances
Product Line:
NetBotz
Environment:
NetBotz version 1
Cause:
Configuration options
Resolution:
User Access Levels for Version 1 Appliances
The Netbotz 300, 303, 310, 400 series appliances have 3 levels of access:
Sensor Access -lets you view camera image and sensor readings only.
Application Access -gives Sensor Access plus ability to view information from any licensed applications (Device Crawlers, Advanced Device Crawlers, or Branch Checker).
Supervisor Access- provides all of the capabilities of the two previous levels plus the ability to change configuration settings and thresholds.
Each access level can be secured with a userid and password.
The user id's and passwords are not transmitted encrypted.
These appliances does not support SSL. If there is a requirement to prevent viewing beyond the user id/pswd security described, it would need to be done through access control with a router or firewall.