Technical FAQs

Ask a Question

Data Purge Rules and Limits for NetBotz 500

Issue:

Data Purge Rules and Limits for NetBotz 500

Product Line:

NetBotz

Environment:

NetBotz 500 NBWL0500

Cause:

Storage Space and Purge specifications.

Resolution:

Appliance Storage Space and Purge Specifications:

- 128MB of RAM

- 60MB is used by the operating system and applications

- 68MB RAM Disk is available for non-persistent storage for:
- Alerts
- Historical sensor readings
- Pictures (for alerts)
- Audio tracks (for alerts)
- Stored data will be kept no longer than 24 hours

- Data purge rules:
- If RAM Disk is full, then oldest data will be deleted to make room for new data
- When age of data reaches 24 hours
- No more than 200 items of any type will be kept (sensor readings, pictures, audio tracks, etc..)
Was this helpful?
What can we do to improve the information ?