Technical FAQs

Ask a Question

TFTPD32.exe no longer bundled in NetBotz firmware download

Issue:

TFTPD32.exe no longer bundled in NetBotz firmware download

Product Line:

NetBotz

Environment:

NetBotz firmware downloads 4.5.1 and after

Cause:

Some antivirus programs see TFTPD32.exe as a vulnerability. In all actuality, it is not however some vulnerabilities may include TFTPD32.exe in order to install themselves but antivirus programs such as McAffee point out that the file itself is not a virus:
http://home.mcafee.com/virusinfo/virusprofile.aspx?key=103882


Resolution:
Due to customer concern, we no longer provide this tftp program with our future downloads. The files used to update using this feature are still available in the download. If you have a tftp program available and wish to use this feature, feel free to do so. If you wish to download the tftpd32.exe program, it is available here:
http://tftpd32.jounin.net/tftpd32_download.html
 
Was this helpful?
What can we do to improve the information ?