Technical FAQs

Ask a Question

Unable to use ISX Central's Auto-Login feature on 3rd party devices.

Issue:
Unable to use ISX Central's Auto-Login feature on 3rd party devices

Product Line:
InfraStruxure Central
StruxureWare Data Center Expert.

Environment:
InfraStruxure CentralAny version
StruxureWare Data Center Expert Any version
3rd party devices.

Cause:
Since 3rd party devices may use login pages or code that differs from APC devices, we have no way to code to each individual device and as such, can not Auto-Login to them.

Resolution:
Auto-Login is only supported for APC devices. APC devices must use version 3.x firmware or above in order to use this feature if an external browser is used.
 
Was this helpful?
What can we do to improve the information ?