Video: How to set up load assist on a Uniflair unit
Issue:
How to set up load assist on a Uniflair unit.
Product line:
Uniflair Gen 1 and Chilled Water Units
Environment:
Uniflair units with push button displays and all Uniflair Chilled Water Units
Cause:
Install, Repair, Maintenance
Resolution:
These are the instructions on how to set up a Uniflair unit to turn on for load assist. Load assist in a Uniflair united is referred to as Sleep Mode. We need to make the proper adjustments to make the unit come on as needed. This operation will only work with two or more units and they must be grouped together.
Press PRG on the display
Press ENTER on Setting Menu
If asked for a pass code 0000 and then ENTER
Press ENTER on Operative Settings
Press the ARROW unit you get to Sleep Mode Settings
Press ENTER to change it from N to Y
Press ENTER to set Min Temp
(This is the temp you want the load assist to stop)
Press the ARROW to change Temp
Press ENTER to move to Max Temp
(This is the temp you want the unit to turn on and help)
Press the ARROW to change Temp
Do the same for Humidity settings
Then press ENTER to go to Fan Cyclical Start
Use the ARROWS to change to Y
Now you have a new line for Cycle Time Min
(This allows the fans to run to keep the air moving after temp or humidity has activated load assist)