Host Name field in NMC web interface returns with "has been entered incorrectly"
Issue
After trying to apply a host name in the web UI of an NMC, an error is returned saying "Host Name (XXXX) has been entered incorrectly." unless there is a "." in the name.
Product Line
Network Management Cards (NMC) - AP9630/AP9631/AP9635
Environment
All serial numbers
AOS v6.1.8
Cause
This was caused by an issue unique to AOS v6.1.8. It has been resolved in later firmware revisions.
Resolution:
Upgrade the firmware of the NMC to the latest revision