Technical FAQs

Ask a Question

Why is the AR7701-S replacing AR7701?

Issue:
The AR7701 had been used to install NetShelter SX cabinets, but that was replaced by AR7701-S.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
A change by IBC required a new seismic bracket.

Resolution:
When IBC updated the seismic standard from seismic zones to Seismic "Areas" it identified areas of more stringent requirements. This prompted an update of our seismic bracket.

 
Was this helpful?
What can we do to improve the information ?