Technical FAQs

Ask a Question

APC UPS Network Management Card (NMC) Compatibility Chart

 

Issue

Which model of UPS Network Management Card is supported in my UPS?


Product Line
 
  • UPS Web/SNMP Card - AP9606

     
  • UPS Network Management Card 1 - AP9617, AP9618, AP9619
     
  • UPS Network Management Card 2 - AP9630/30CH, AP9631/31CH, AP9635/35CH
     

Environment
  • All firmware versions (unless otherwise specified)
  • All serial numbers

Cause

This compatibility chart has been created for reference.


Resolution

Please refer to the table below.

Note: Some of these management cards are older and discontinued. This means while there may be some compatibility between current UPS models and discontinued management cards, support for new device features or management card features and bug fixes will only be available with the current generation of Network Management Card for your device. Current generation Network Management Cards purchased on their own will ship with the SUMX application file, for use with the SmartUPS family. Firmware files for use in other UPS systems can be found here: http://www.apc.com/us/en/tools/download/
 
Network Management Card Model(s) UPS Model Note(s)
  • AP9617, AP9618, AP9619
  • Single and Three Phase Smart-UPS with the following model prefixes:
    • SU
    • SUA
    • SUM
    • SURT
    • SURTA
    • SURTD
    • SUVT*
  • Matrix UPS with UPS firmware versions Y or Z
    • MX3000
    • MX5000
  • Single phase Symmetra models:
    • Symmetra Power Array
    • Symmetra RM 6K/12K
    • Symmetra LX
  • Three phase Symmetra models:
    • 20kW Symmetra PX All-In-One
    • 40kW Symmetra PX
    • 80kW Symmetra PX
    • 100kW Symmetra PX2**
    • 160kW Symmetra PX2**
  • Silcon
  • *Note: SUVT model UPSs with v7.X.X firmware should use NMC2 to take advantage of all UPS firmware enhancements.
 
  • **Note: This add-on option is only able to monitor the UPS, and not any power distribution. The embedded NMC within the UPS must be used to monitor any power distribution.
  • AP9630/30CH, AP9631/31CH
  • Single and Three Phase Smart-UPS with the following model prefixes:
    • SU
    • SUA
    • SUM
    • SURT
    • SURTA
    • SURTD
    • SUVT & MGE Galaxy 3500
    • SMT
    • SMX
    • SRT
  • Matrix UPS with UPS firmware versions Y or Z
    • MX3000
    • MX5000
  • Single phase Symmetra models:
    • Symmetra Power Array
    • Symmetra RM
    • Symmetra LX
  • Three phase Symmetra models:
    • 48kW Symmetra PX2 All-In-One*
    • 20kW Symmetra PX
    • 40kW Symmetra PX
    • 80kW Symmetra PX
    • 100kW Symmetra PX2*
    • 160kW Symmetra PX2*
  • SMX/SMT require sumx APP v5.0.3 or higher.
 
  • SRT models require sumx APP v6.0.7, or v6.2.0 or higher
 
  • *Note: This add-on option is only able to monitor the UPS, and not any power distribution. The embedded NMC within the UPS must be used to monitor any power distribution.
  • AP9630/30CH, AP9631/31CH, AP9635/35CH
  • Three Phase Galaxy UPS units
    • ​Galaxy 300/7000*
    • Galaxy VM
  • *Ships with AP9630 pre-installed in units manufactured post 2012. Older G7000 models require a special upgrade kit pre-2012 manufacture date.
  • AP9635/35CH
  • 3 Phase UPS models including:
    • Symmetra PX 250/500
    • SUVT/G500*
  • Single Phase UPS models including:
    • SmartUPS*
    • Symmetra*
  • *With AOS 6.4+ only
  • G5K9635CH
  • MGE Galaxy 5000
  • Kit includes all necessary parts to install an AP9635 for all G5000 UPS serial numbers and firmwares.
  • G9K9635CH
  • MGE Galaxy 9000
  • Kit includes all necessary parts to install an AP9635 for all G9000 UPS serial numbers and firmwares.
  • AP9606
  • Older UPS models including:
    • Smart-UPS with the following model prefix:
      • SU
      • SUA
    • Symmetra Power Array
    • Symmetra RM 6K/12K
    • Matrix UPS with UPS firmwares Y or Z
      • MX3000
      • MX5000
    • 40kW Symmetra PX
    • 80kW Symmetra PX
  • Silcon
 
  • 0J-0N-9581GVM
  • Galaxy VM
  • Spare part for Galaxy VM Display/Embedded Network Management Card inside
  • 0G-9354
  • W0G-9354 (spare part)
  • Three phase Symmetra (PX2) models:
    • 48kW Symmetra PX All-In-One
    • 100kW Symmetra PX
    • 160kW Symmetra PX
  • UPS brain with embedded Network Management Card.


 
Was this helpful?
What can we do to improve the information ?