Technical FAQs
Technical FAQs
Issue:
Customers may want to install a PDU in the opposite direction that it would normally be installed.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Customers may want to install the 0U PDU with the power supply cord facing either the top or bottom of the cabinet depending upon their preference, even if this causes the display to be upside down.
Resolution:
All APC by Schneider Electric brand 0U PDUs are designed to be installed into a NetShelter SX cabinet in either direction, with the supply cord facing up or down.