Technical FAQs

Ask a Question

Tips For Installing PowerChute Network Shutdown - more than 50 Servers Connected

Issue:
How to have configure PowerChute Network Shutdown with more that 50 computers connected to one UPS?

Product Line/s:
PowerChute Network Shutdown
AP9617, AP9618, AP9619, AP9630, AP9631, AP9635

Environement:
All supported OS

Cause:
Installation information

Solution:

Please review Application Note AN-101 v2 http://www.apcmedia.com/salestools/BKIR-6QWKC5/BKIR-6QWKC5_R2_EN.pdf
Was this helpful?
What can we do to improve the information ?