Technical FAQs

Ask a Question

Symmetra PX1-PX2; How to interpret the loading displayed in Symmetra PX


 
 
Issue:
How to interpret the loading displayed in Symmetra PX 
 
Product line:
Symmetra PX1-PX2
 
Environment:
All models, all serial numbers
 
Cause:
 The opening screen of Powerview shows loading of the heavily loaded phase in Symmetra PX.
 


Resolution:
Typical loading data from Symmetra PX unit is give below as an example

When Powerview opening screen showed “loading 24%”, the actual loading on each of the phases recorded in powerview is as below
 
Phase
Loading in KVA
Current in Amps
% loading per phase
L1
0.93
3A
13%
L2
1.66
6A
24%
L3
0.67
2A
10%
 
As seen from the above example the front screen shows the highest loaded phase and not average as commonly interpreted by many customers




Was this helpful?
What can we do to improve the information ?