Technical FAQs

Ask a Question

Video: How to clear active alarms on an InRow ACRD60xx

Issue:
Active alarms present on unit.

Product line: 
InRow RD ACRD600, ACRD600P, ACRD601, ACRD601P.
 
Environment: 
All Serial Numbers.
 
Resolution:
  1. Press the flashing X to view active alarms.
  2. Press Clear to clear the active alarms. A confirmation screen is displayed.
  3. Enter the Admin password to erase the alarms list.
  4. Select Yes to erase all of the alarms. Select No to return to the Active Alarms screen.

Was this helpful?
What can we do to improve the information ?